Edmund Optics® (EO), the premier provider of optical components, announces that customers in China now have direct access to over 1,600 high performance laser optics from Edmund Optics’ large inventory of stock optics ready for immediate delivery. In addition, custom design and manufacturing of laser optics is now being offered for the first time to meet growing customer needs.
Exceptional quality and performance
“Our high quality, high precision optics meet the performance requirements of China’s growing laser market since they are designed and manufactured to the most rigorous specifications, thereby ensuring repeatability in the most demanding applications,” states Timothy Paul Kennedy, Sales Director, Asia. “Whether it’s a researcher needing immediate delivery on a small-quantity order or an industrial OEM looking for a quick modification to one of our standard products, Edmund Optics’ vast inventory provides customers exceptionally fast turnaround.”
Products now available for purchase in China include Edmund Optics’ new TECHSPEC® High Power Nd:YAG Laser Mirrors and TECHSPEC® Variable Beam Expanders. The laser mirrors feature industry-leading, all-dielectric Ion Beam Sputtered (IBS) coatings to deliver high damage thresholds and up to 99% reflectivity for demanding applications in high power beam delivery and laser beam steering, while the versatile variable beam expanders offer continuous magnification for high power laser applications like prototyping or research and development, which may require magnification changes.
Top-tier customer service
Dr. Jeremy Chang, VP of Asia Operations, adds, “When customers from China purchase their laser optical components directly from Edmund Optics, not only do they benefit from excellent product quality and short lead-times, but they can also receive assistance from our team of highly-skilled sales and technical support specialists in their local time zones and native language.”
Edmund Optics’ laser optics, including the TECHSPEC High Power Nd:YAG Laser Mirrors and TECHSPEC Variable Beam Expanders, will be demonstrated at CIOE 2015, the China International Optoelectronic Expo Hall 9 Booth 9I10 , Shenzhen Convention and Exhibition Center from 31st August through 3rd September, 2015.