The polarization of light is changed when it is incident on a beamsplitter oriented at 45 degrees. For randomly polarized input light, the S-polarization state is reflected more than the average amount of reflection and the P-polarization state is reflected less than the average. Plate beamsplitters are very sensitive to polarized light, the transmission of the S- and P-polarization states can each vary typically as much as 20% from the average at 550nm for a visible spectrum coating. Our dichroic cube beamsplitters are also extremely sensitive to polarization. The S- and P-polarization states can have a difference as large as 70%, while each differing from the average transmission by approximately 20-30%. Beamsplitters should be selected carefully prior to integration into polarization sensitive applications. We do offer polarized cube beamsplitters that offer 92% reflection for S-polarization at 632.8nm.
ou consulter les numéros d’autres pays
facile à utiliser
entrer les numéros de stock pour commencer
Copyright 2023 | Edmund Optics, Ltd Unit 1, Opus Avenue, Nether Poppleton, York, YO26 6BL, UK
L'entreprise Edmund Optics GmbH en Allemagne agit comme un mandataire d'Edmund Optics Ltd au Royaume-Uni. Le titulaire du contrat est Edmund Optics Ltd au Royaume-Uni.