Produit ajouté au panier

Edmund Optics®

Centre de Connaissance

 Une bibliothèque vérifiée de ressources techniques fiables créées par nos 240+ ingénieurs internationaux.

Filtre
Search Results for: Prismes Laser (98)

Paires de prismes anamorphiques

Anamorphic prism pairs circularize elliptical laser beams, which results in smaller focused spot sizes.

View Now Add to saved content

Diagrammes de tunnel de prismes

View Now Add to saved content

Aperçu du modelage de faisceaux laser

Apprenez à évaluer les options de modelage du profil d'irradiation et de la phase des faisceaux laser ✓ Maximisez les performances de système.

View Now Add to saved content

Matériaux d’optique laser usuels

Understanding the most commonly used laser optics materials will allow for easy navigation of EO’s wide selection of laser optics components.

View Now Add to saved content

Modes de résonateurs laser

The length of a laser resonator determines the laser’s resonator modes, or the electric field distributions that cause a standing wave in the cavity.

View Now Add to saved content

L’absorption en optique laser

Light is absorbed in optical media through several methods including exciting electrons to higher energy states and converting to thermal energy

View Now Add to saved content

Traitements AR pour un Seuil d'Endommagement Laser Élevé

Traitements AR pour un Seuil d'Endommagement Laser Élevé - En savoir plus !

View Now Add to saved content

Expanseurs de faisceau laser

Laser beam expanders are critical for reducing power density, minimizing beam diameter at a distance, and minimizing focused laser spot size.

View Now Add to saved content

Métrologie pour les optiques laser

Metrology is critical for ensuring that optical components consistently meet their desired specifications, especially in laser applications.

View Now Add to saved content

Densité de puissance laser versus densité d'énergie laser

Rappelez-vous les concepts de la densité de puissance et la densité d'énergie, la fluence et l'irradiance dans les applications de l'optique laser. Allez-y.

View Now Add to saved content

Paramètres clés d’un système laser

Learn the key parameters that must be considered to ensure you laser application is successful. Common terminology will be established for these parameters.

View Now Add to saved content

Introduction aux prismes optiques

Learn about the different types of optical prisms, their applications, and how to select the right prism for your specific system.

View Now Add to saved content

Comprendre et Spécificier le LIDT des Composants Laser

Laser induced damage threshold (LIDT) denotes the maximum laser fluence an optical component can withstand with an acceptable amount of risk.

View Now Add to saved content

Essais de détermination du seuil de dommage laser

Testing laser induced damage threshold (LIDT) is not standardized, so understanding how your optics were tested is critical for predicting performance.

View Now Add to saved content

Guide pour spécifier (sans surspécifier) les pertes en optique laser

Surspécifier les pertes optiques dans les systèmes laser n'améliorera pas davantage vos performances, mais pourrait vous coûter plus d'argent.

View Now Add to saved content

Dommages volumiques causés par le laser dans le verre

Learn why the bulk laser-induced damage threshold (LIDT) of glass is significantly different than the LIDT optical components with coatings, such as AR thin films.

View Now Add to saved content

L'importance de la polarisation dans les applications laser

Edmund Optics explique la polarisation laser avec son un impact sur la réflectance, la focalisation du faisceau et d'autres comportements clés.

View Now Add to saved content

Pourquoi utiliser un faisceau laser à intensité uniforme

Convertir un profil de faisceau laser gaussien en un profil à intensité uniforme peut avoir de nombreux avantages. En savoir plus chez Edmund Optics.

View Now Add to saved content

Effets de la planéité de la surface de miroirs laser

View Now Add to saved content

L’importance du diamètre du faisceau pour le seuil de dommage laser

Le diamètre d'un laser affecte fortement le seuil de dommage induits par le laser (LIDT) d'un composant optique, car le diamètre du faisceau influence directement la probabilité qu’un endommagement induit par le laser se produise.

View Now Add to saved content

Imagerie par Fluorescence Illuminée au Laser

Fluorescence imaging systems are composed of three major components, an illumination source, a photo-activated fluorophore sample, and detector.

View Now Add to saved content

Miroirs hautement dispersifs

Ultrafast highly-dispersive mirrors are critical for pulse compression and dispersion compensation in ultrafast laser applications, improving system performance.

View Now Add to saved content

Que sont les Séparateurs de Faisceau ?

Les séparateurs de faisceau sont des composants optiques utilisés pour séparer la lumière incidente en deux faisceaux distincts selon un rapport déterminé.

View Now Add to saved content

Guide de sélection des polariseurs

Le guide de sélection des polariseurs d'Edmund Optics permet d'affiner votre recherche d'un type spécifique de polariseur.

View Now Add to saved content

Utiliser des Composants à Monture C avec le Système de Cage Optique

Choisir le bon composant de fixation pour optimiser la performance d’un système optique - EO offre des montures pour toute une gamme de composants optiques.

View Now Add to saved content

Les principes fondamentaux de la diffusion et de la spectroscopie Raman

✓ Utilise une nappe laser 2D pour éclairer une fine tranche de l'échantillon et exciter la fluorescence. ✓ Réduise phototoxicité et dommages.

View Now Add to saved content

Silice Fondue indice UV ou IR

La silice fondue est souvent le matériau préféré en imagerie de précision en raison de ses performances optiques constantes et reproductibles.

View Now Add to saved content

Tout savoir sur les réseaux de diffraction

Découvrez les différents réseaux de diffraction, comment ils séparent la lumière incidente en faisceaux distincts et comment choisir le meilleur réseau.

View Now Add to saved content

Traitements Antireflets (AR)

Les traitements antireflets (AR) sont appliqués aux composants optiques afin d'augmenter le débit et de réduire les risques causés par les reflets.

View Now Add to saved content

Comprendre les spécifications optiques

Do you want to know more about the importance of optical specifications? Learn the different types of specifications and their impact on your system at Edmund Optics.